Suchbegriff

Start of the DTM season: Schaeffler forges ahead with technology transfer

Pressrelease Stage Image
Marco Wittmann has his sights set on the title with the Green Machine.

30.07.2020 | Herzogenaurach

  • Successful cooperation enters second year
  • Schaeffler using partnership with BMW M Motorsport to gain knowledge from the DTM, in order to use it in production development
  • Matthias Zink: “The goal is to win the title with Marco Wittmann.”

This weekend, the new season of the German Touring Car Masters (DTM) gets underway at Spa-Francorchamps in Belgium. Global automotive and industrial supplier, Schaeffler, is using the racing series to test technology under extreme conditions and to ensure it is ready for production. “The optimization of the combustion engine continues to play an important role for Schaeffler,” says Matthias Zink, CEO Automotive OEM at Schaeffler. “The DTM and our intense partnership with BMW M Motorsport provide valuable insights for Schaeffler.”

Focus remains on technology transfer
The know-how gained on the motorsport scene is incorporated directly in the development of components and systems, ensuring the highest possible degree of quality and reliability. The combustion engine still has great potential. For this reason, Schaeffler is continuing to concentrate on combustion engines and gearboxes, as well as electromobility. The goal is to increase their efficiency and to provide Schaeffler’s customers with tailored solutions through innovative products like the Thermal Management Module (TMM), the fully-variable UniAir valve control system and the electric camshaft timer.

Successful partnership enters its second year
Following the successful debut of the premium partnership between Schaeffler and BMW M Motorsport in the DTM, Marco Wittmann and the BMW M4 DTM – adorned in the typical Schaeffler colours of green and white – are now set for their second season together. “The team has done its homework over the winter. Our goal is to win the title with Marco Wittmann in our second season together,” says Matthias Zink. Postponements due to the COVID-19 pandemic mean the DTM calendar has had to be adapted to the new circumstances. 18 races will take place within the space of just three months and seven days. Only with comprehensive safety and hygiene measures in place for teams and drivers, as well as races held behind closed doors, has it been possible to get the series up and running this year. Even for two-time DTM champion Marco Wittmann, it is going to be a completely new experience: “I am really looking forward to my second season in the Schaeffler BMW M4 DTM, although it is going to be totally different to anything we have experienced before. I will definitely miss the fans, but am optimistic about the future and ready to challenge for the title.”

Herausgeber: Schaeffler AG
Ausgabeland: Deutschland

Zugehörige Medien

Nutzungsbedingungen für Schaeffler-Pressebilder

Schaeffler-Pressebilder dürfen ausschließlich für redaktionelle Zwecke verwendet werden. Sofern nichts anderes angegeben, liegen sämtliche Urheber-, Nutzungs- und Verwertungsrechte bei der Schaeffler Technologies AG & Co. KG, Herzogenaurach, oder bei einem ihrer verbundenen Unternehmen. Die Vervielfältigung und die Veröffentlichung der Schaeffler-Pressebilder ist nur mit Angabe der Quelle wie folgt „Bild: Schaeffler“ gestattet. In diesem Fall ist die Verwendung honorarfrei möglich. Die Befugnis zur Verwendung zu werblichen oder sonstigen kommerziellen Zwecken, insbesondere zur kommerziellen Weitergabe an Dritte, wird hiermit nicht eingeräumt. Bearbeitungen bedürfen in jedem Fall der Zustimmung von Schaeffler.

Bei Veröffentlichung von Schaeffler-Pressebildern in Printmedien bitten wir um die Zusendung eines Belegexemplars (bei Veröffentlichung in elektronischen Medien um ein digitales Exemplar bzw. einen Link). Bei Verwendung von Schaeffler-Pressebildern in Filmen bitten wir um Benachrichtigung und Angabe des Filmtitels.

Die Nutzung der Schaeffler-Pressebilder unterliegt deutschem Recht mit Ausnahme des Kollisionsrechts, Gerichtsstand ist Nürnberg, Deutschland.
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
Schaeffler verwendet Cookies, um Ihnen eine optimale Nutzung zu gewährleisten. Durch die weitere Nutzung dieser Website stimmen Sie der Verwendung von Cookies zu. Weitere Informationen

Akzeptieren