Suchbegriff

Innovative components for lightweight and collaborative robots For maximum load-carrying capacity and rigidity: XZU conical thrust cage needle roller bearing and RTWH gearbox from Schaeffler

Pressrelease Stage Image
The new XZU conical thrust cage needle roller bearing by Schaeffler is used in lightweight and collaborative robots both as an articulated arm bearing and as a main bearing support for Schaeffler’s new RTWH precision gearbox.

12.02.2020 | Schweinfurt/Hannover

  • Schaeffler develops new market with major growth potential
  • New XZU conical thrust cage needle roller bearing for robot and cobot joints: 20 percent less friction and 30 percent greater rigidity
  • New RTWH precision gearbox for compact design envelope

Today’s advanced automation and production facilities need lightweight robots (LWRs) and collaborative robots (cobots) that are highly dynamic and accurate. Drawing on its many years of experience in industrial automation, Schaeffler has developed two new and highly innovative components for LWRs and cobots, with which it is opening up new opportunities in a fast-growing market segment.

The new XZU conical thrust cage needle roller bearing is used both as an articulated arm bearing in LWRs and cobots and as the main bearing support for the company’s new RTWH precision gearbox. This combination of RTWH gearbox and XZU bearing ensures the most compact design envelope and the greatest rigidity possible in application.

XZU conical thrust cage needle roller bearing for articulated-arm bearing supports
Schaeffler’s double-row conical thrust cage needle roller bearing is the culmination of 70 years of experience in the design and manufacture of needle roller bearings. The main benefit of the bearing for customers is that it has more load-bearing rolling elements than the crossed roller bearings currently used for articulated-arm bearing supports while maintaining the same design envelope. Customers thus have the option of using smaller-sized bearings, thereby saving on space and weight – major benefits when it comes to downsizing. This opens up new opportunities and possibilities in the development of LWRs and cobots. The bearing technology spells a constantly growing array of new applications for users.

Apart from more load-bearing rolling elements, the XZU unit’s X arrangement of needle rollers in two raceways offers support distances that, depending on installed size, increases rigidity by at least 30 percent compared with crossed roller bearings. What is more, by housing the rolling elements in cage guides and having them configured in two raceways instead of just one, the XZU delivers a 20 percent reduction in friction.

For customers, this all translates into more precise movement and less overshoot on reaching the end position. Overall, applications using these bearings require fewer control processes and can operate at higher speeds, thereby making the production cycle in question much more efficient.

RTWH precision gearbox – silk hat-type speed reducer
Schaeffler offers ready-to-install silk hat-type speed-reduction gears – or “speed reducers”, as they are also known – for use in robot articulated joints. By harnessing the functional principles of strain wave gearing, the RTWH combines high gear ratios – and correspondingly high torques – with relatively lightweight construction. The RTWH precision gearbox developed by Schaeffler is characterized by clearance-free operation, high positioning accuracy, and compactness. It is also very durable and therefore has a long operating life.

A long operating life is a key factor in robots, which need to operate with a maximum of reliability and a minimum of downtime. Depending on their size, Schaeffler’s RTWH gearboxes can deliver reduction ratios of 50:1 to 150:1. The torques resulting from these reductions are transmitted reliably and accurately thanks to the gearbox’s robust construction and the integration of the highly rigid XZU conical thrust cage needle roller bearing. As a result, robots fitted with RTWH gearboxes are highly efficient and able to move through to their end positions dynamically, accurately, and without excessive overshoot. This means they are able to complete sorting, handling, and assembly tasks quickly and efficiently.

Another stand-out feature of the new precision gearbox from Schaeffler is its compact and maintenance-free design. It is available in all standard sizes. The drive flange is a hollow shaft and can be factory-tailored to the customer’s requirements.

Herausgeber: Schaeffler Technologies AG & Co. KG
Ausgabeland: Deutschland

Zugehörige Medien

Nutzungsbedingungen für Schaeffler-Pressebilder

Schaeffler-Pressebilder dürfen ausschließlich für redaktionelle Zwecke verwendet werden. Sofern nichts anderes angegeben, liegen sämtliche Urheber-, Nutzungs- und Verwertungsrechte bei der Schaeffler Technologies AG & Co. KG, Herzogenaurach, oder bei einem ihrer verbundenen Unternehmen. Die Vervielfältigung und die Veröffentlichung der Schaeffler-Pressebilder ist nur mit Angabe der Quelle wie folgt „Bild: Schaeffler“ gestattet. In diesem Fall ist die Verwendung honorarfrei möglich. Die Befugnis zur Verwendung zu werblichen oder sonstigen kommerziellen Zwecken, insbesondere zur kommerziellen Weitergabe an Dritte, wird hiermit nicht eingeräumt. Bearbeitungen bedürfen in jedem Fall der Zustimmung von Schaeffler.

Bei Veröffentlichung von Schaeffler-Pressebildern in Printmedien bitten wir um die Zusendung eines Belegexemplars (bei Veröffentlichung in elektronischen Medien um ein digitales Exemplar bzw. einen Link). Bei Verwendung von Schaeffler-Pressebildern in Filmen bitten wir um Benachrichtigung und Angabe des Filmtitels.

Die Nutzung der Schaeffler-Pressebilder unterliegt deutschem Recht mit Ausnahme des Kollisionsrechts, Gerichtsstand ist Nürnberg, Deutschland.
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
Schaeffler verwendet Cookies, um Ihnen eine optimale Nutzung zu gewährleisten. Durch die weitere Nutzung dieser Website stimmen Sie der Verwendung von Cookies zu. Weitere Informationen

Akzeptieren