Suchbegriff

From driver assistance systems through to comfort functions: One control unit does it all Getting connected for an autonomous future

Pressrelease Stage Image
The XTRONIC Control Unit combines a range of interlinked and integrated components. The control unit is fully independent of vehicle platform type.

12.09.2019 | Herzogenaurach/Frankfurt

  • Schaeffler presents its innovative XTRONIC Control Unit as a basis for autonomous driving
  • The Control Unit is not dependent on any specific platform, and it ensures a comprehensive range of safety, monitoring, operating, and comfort functions
  • The solution is in volume production for several global OEMs

Remote monitoring and control are especially important for autonomous vehicles. However, such functions have thus far only been available in isolated systems or else have been dependent on specific platforms. The XTRONIC Control Unit on the other hand combines safety, monitoring, operating, and comfort functions in a single system. The innovative system also makes a convincing case thanks to its wide range of interlinked, integrated components – from entertainment systems through to condition monitoring for vehicle components. The reliable interlinking of innovative driver assistance systems together with radar, lidar, ultrasound, and even artificial intelligence thus provides the technological basis for autonomous driving.

Integration across platforms

The XTRONIC Control Unit allows digital control and monitoring to be combined in a single application for smartphones, tablet PCs, and smartwatches. The most important data are thus always available in the cloud and can be accessed from anywhere via mobile device. It doesn’t matter what type of vehicle platform is used for the implementation of the connectivity tools based on the control unit. Applications include not only (partly) autonomous vehicles but also commercial vehicles and motorhomes. The control unit recently went into volume production for several global OEMs to use in these fields of application.

CampConnect – the digital control system for campervans

At the IAA, Schaeffler will be demonstrating the advantages of this system using a campervan as an example. “CampConnect” is based on the XTRONIC Control Unit and allows comfort and safety functions in campervans and caravans to be digitally controlled. For example, end customers can access the full range of control functions and carry out status checks via smartphone while they are on the move. The owner can thus check the fuel level and the temperature, for example. Condition monitoring and predictive maintenance of components ensure availability and provide the basis for intelligent maintenance planning for both vehicles and entire vehicle fleets. If a break-in attempt occurs, an alarm is also immediately sounded.

About XTRONIC

XTRONIC has been part of Schaeffler since May 2019 and, as a technology partner, develops customized software and electronics solutions for the international automotive industry. The company’s service portfolio includes applications that range from automated driving and electric mobility through to functional safety as well as methods, tools, and testing systems – all of which makes XTRONIC a specialist when it comes to innovative interlinking for vehicles.

Herausgeber: Schaeffler AG
Ausgabeland: Deutschland

Zugehörige Medien

Nutzungsbedingungen für Schaeffler-Pressebilder

Schaeffler-Pressebilder dürfen ausschließlich für redaktionelle Zwecke verwendet werden. Sofern nichts anderes angegeben, liegen sämtliche Urheber-, Nutzungs- und Verwertungsrechte bei der Schaeffler Technologies AG & Co. KG, Herzogenaurach, oder bei einem ihrer verbundenen Unternehmen. Die Vervielfältigung und die Veröffentlichung der Schaeffler-Pressebilder ist nur mit Angabe der Quelle wie folgt „Bild: Schaeffler“ gestattet. In diesem Fall ist die Verwendung honorarfrei möglich. Die Befugnis zur Verwendung zu werblichen oder sonstigen kommerziellen Zwecken, insbesondere zur kommerziellen Weitergabe an Dritte, wird hiermit nicht eingeräumt. Bearbeitungen bedürfen in jedem Fall der Zustimmung von Schaeffler.

Bei Veröffentlichung von Schaeffler-Pressebildern in Printmedien bitten wir um die Zusendung eines Belegexemplars (bei Veröffentlichung in elektronischen Medien um ein digitales Exemplar bzw. einen Link). Bei Verwendung von Schaeffler-Pressebildern in Filmen bitten wir um Benachrichtigung und Angabe des Filmtitels.

Die Nutzung der Schaeffler-Pressebilder unterliegt deutschem Recht mit Ausnahme des Kollisionsrechts, Gerichtsstand ist Nürnberg, Deutschland.
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
Schaeffler verwendet Cookies, um Ihnen eine optimale Nutzung zu gewährleisten. Durch die weitere Nutzung dieser Website stimmen Sie der Verwendung von Cookies zu. Weitere Informationen

Akzeptieren