Suchbegriff

Schaeffler champions autonomous driving in China

Pressrelease Stage Image
Signing ceremony for an investment agreement aimed at supporting and facilitating autonomous driving in China: Matthias Zink (third from left), CEO Automotive OEM at Schaeffler AG and Hu Zhongxiong, Mayor of Changsha (second from right) during the signing ceremony in the presence of German Chancellor Dr. Angela Merkel and Chinese Premier Li Keqiang. (Image: German Federal Government/Steffen Kugler)

06.09.2019 | Herzogenaurach/Peking

  • Research and development milestone for Space Drive drive-by-wire system and the Schaeffler Mover
  • Schaeffler signs investment agreement with China’s Hunan province during a state visit to China by German Chancellor Angela Merkel
  • Schaeffler to establish new R&D center to support the creation of a complete ecosystem for autonomous driving in the city of Changsha and surrounding region

Schaeffler, a leading global automotive and industrial supplier, has signed an investment agreement with China’s Hunan province in a move aimed at supporting and facilitating autonomous driving in China using Schaeffler technologies. Under the agreement, both parties will jointly develop a mobility ecosystem for intelligent vehicles in the provincial capital of Changsha. Schaeffler’s role in the venture will revolve mainly around the further development of its Space Drive technology, a key enabler of autonomous driving, and the Schaeffler Mover, a mobility concept featuring Schaeffler Intelligent Corner Module technology. The formal signing ceremony for the agreement was held in Beijing and was attended by German Chancellor Angela Merkel and Chinese Premier Li Keqiang.

The agreement was signed by Matthias Zink, Schaeffler’s CEO Automotive OEM, and Hu Zhongxiong, the Mayor of Changsha, a city of seven million people in Hunan Province, and Secretary of the CPC Hunan Xiangjiang New Area Working Committee. It opens the way for the establishment in Hunan Xiangjiang New Area of a local Schaeffler company to implement Schaeffler’s Space Drive drive-by-wire technology locally in Hunan province and take the Schaeffler Mover platform forward into the next phase of its development. The establishment of the new company is further testimony that Schaeffler’s technologies and products for intelligent vehicles are ideally suited to use in big cities, not least China’s major areas of conurbation.

Space Drive and Schaeffler Mover featuring Intelligent Corner Modules
Space Drive is a key enabling technology for tomorrow’s automated, autonomous and connected vehicles that is currently being developed with a view to volume production. It is a leading drive-by-wire technology comprising a triple-redundant electronic interface that operates vehicle steering, accelerator and braking functions by wire, rather than mechanical means. As such, it enables autonomous driving in a wide range of application scenarios. Space Drive is the world’s first – and so far only – drive-by-wire system to be licensed for on-road use and to feature the level of redundancy needed to guarantee functional safety and reliability.

Among its many applications, Space Drive is used in the all-electric Schaeffler Mover, which was recently awarded the German Mobility Prize by Germany’s Federal Ministry for Transport and Digital Infrastructure. The Schaeffler Mover is a flexible and locally zero-emission platform that supports a wide range of vehicle concepts. Schaeffler uses it to test and demonstrate tomorrow’s innovative drive train and chassis technologies. The Schaeffler Mover integrates all the components needed for driving functionality – drive system, battery, braking system and steering – in a compact unit known as a rolling chassis. The drive system is based on Schaeffler’s proprietary Intelligent Corner Module technology, which supports a steering angle of up to 90 degrees. The Schaeffler Mover platform is a particularly attractive solution for urban mobility because it supports a range of superstructures and can thus be used in a range of applications, from robotaxi to autonomous delivery vehicle. Schaeffler will be showcasing its Space Drive Technology and its Schaeffler Mover/Schaeffler Intelligent Corner Module combo at the International Motor Show (IAA) in Frankfurt, Germany, opening next Tuesday.

New R&D center in Hunan region
Alongside all of this, Schaeffler is planning to set up a new R&D facility in Hunan province. It will be the second R&D center operated by Schaeffler Greater China and its focus will be on developing technologies for tomorrow’s intelligent vehicles. With the support of local government authorities, the new R&D center will partner with other providers of autonomous driving technologies to create an entire value chain for intelligent vehicles, complete with supporting industrial ecosystem.

“China is a major market for Schaeffler, and we have every confidence that it will continue to grow,” commented Schaeffler CEO Automotive OEM Matthias Zink. “We want to be close to market so that we can give our customers in China access to top-quality products and services. With that in mind, we will continue our investment in R&D, grow our local market presence also in Greater China and help develop the industrial base for intelligent, connected vehicles.”

Herausgeber: Schaeffler AG
Ausgabeland: Deutschland

Zugehörige Medien

Nutzungsbedingungen für Schaeffler-Pressebilder

Schaeffler-Pressebilder dürfen ausschließlich für redaktionelle Zwecke verwendet werden. Sofern nichts anderes angegeben, liegen sämtliche Urheber-, Nutzungs- und Verwertungsrechte bei der Schaeffler Technologies AG & Co. KG, Herzogenaurach, oder bei einem ihrer verbundenen Unternehmen. Die Vervielfältigung und die Veröffentlichung der Schaeffler-Pressebilder ist nur mit Angabe der Quelle wie folgt „Bild: Schaeffler“ gestattet. In diesem Fall ist die Verwendung honorarfrei möglich. Die Befugnis zur Verwendung zu werblichen oder sonstigen kommerziellen Zwecken, insbesondere zur kommerziellen Weitergabe an Dritte, wird hiermit nicht eingeräumt. Bearbeitungen bedürfen in jedem Fall der Zustimmung von Schaeffler.

Bei Veröffentlichung von Schaeffler-Pressebildern in Printmedien bitten wir um die Zusendung eines Belegexemplars (bei Veröffentlichung in elektronischen Medien um ein digitales Exemplar bzw. einen Link). Bei Verwendung von Schaeffler-Pressebildern in Filmen bitten wir um Benachrichtigung und Angabe des Filmtitels.

Die Nutzung der Schaeffler-Pressebilder unterliegt deutschem Recht mit Ausnahme des Kollisionsrechts, Gerichtsstand ist Nürnberg, Deutschland.
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
Schaeffler verwendet Cookies, um Ihnen eine optimale Nutzung zu gewährleisten. Durch die weitere Nutzung dieser Website stimmen Sie der Verwendung von Cookies zu. Weitere Informationen

Akzeptieren